11/30/2022 8:35 PM | |
Joined: 12/17/2019 Last visit: 4/6/2024 Posts: 33 Rating: (1) |
dear all expert hope reply on my enquiry use tia portal 15.1v , cpu 1214DC/DC/DC , encoder OMRON / NPN / 100kHz , 1000 P/R , my enquiry that when counting equal target pulse as example 30000 should set bit our create out but signal what ever you need . the issue that pulse pass the equal target without do any out signal it's reach 30300 but before this pulse when equal 30000 most PLC cycle fast read so can catch this signal and do the requirement . notice input signal filter for i0.0 and i0.1 are 0.8 microsecond any try 0.1 microsecond but still same issue how can solve that issue so can work on exact target pulse . please check attached file . best regards. Attachmentencoder.pdf (258 Downloads) |
Last edited by: muntadher at: 11/30/2022 20:47:58 |
|
Follow us on