11/23/2022 4:30 AM | |
Joined: 10/23/2015 Last visit: 6/10/2024 Posts: 29 Rating: (0) |
Dear Support, I’m working on WinCC V7.5, Server-Client Configuration. In the user administrator, I created the users for login in server project PC and displayed which user as login from the startscreen. When I login from server PC, the logged user is working fine and showing the logged user in both server & client PCs. Then, I export the file from “User Administrator” in txt format from server pc and imported the file in the Client PC. Copy the C script from the server project to Client project folder of the same name. (From “Project name > Library” folder). I refer to the user manual and try out. But when I logged from Client PC, logged user able to login but unable to display on the startscreen. Refer to the attachment and advise. BR Aravind AttachmentUserLogin-WinCC-V7.5.docx (333 Downloads) |
Follow us on