12/9/2022 11:12 AM | |
Joined: 12/8/2022 Last visit: 12/11/2022 Posts: 1 Rating: (0) |
Hi, I replaced CU card by CUVC in a simovert inverter could you please to help me what are the parameters needed to join the cuvc card with the PLC because I have a problem with the Communication that is the green light of CB card is going off Also No fault appeares on the PMU the PLC gives BF fault The address on P918. 1 is right. Please advise Thanks Ali Hussein Abo Bakr ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 12/09/2022 14:40:10New subject after splitting |
|
Follow us on