8/11/2020 10:28 AM | |
Joined: 2/6/2020 Last visit: 3/11/2024 Posts: 23 Rating: (0) |
Hello, I have problem. During VPN connection, I can see all items, plc, inverters and hmi in VPN router. I can connect to plc and inverters through VPN, but can't connect to hmi. Then I do search accesible devices in TIA portal, I see all except hmi. Connected VPN router directly to hmi, start online search, it shows that 0 devices accessible. I done ping and it shows OK. First time I got that HMI not shown as accesible device as PLC is accesible. During commissioning at the customer I had no problem to connect to HMI directly. Any ideas? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/11/2020 10:50:46New subject after splitting |
|
11/8/2020 1:01 AM | |
Posts: 1 Rating: (0) |
I have the same problem, I changed the route address of the Hmi to the VPN address but doesn't work |
12/15/2022 12:06 PM | |
Joined: 8/3/2009 Last visit: 4/26/2024 Posts: 12869 Rating: (1641)
|
Hello do you already have tried this: https://support.industry.siemens.com/cs/ww/en/view/109781206 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on