12/30/2020 4:37 PM | |
Joined: 12/18/2014 Last visit: 6/1/2024 Posts: 33133 Rating: (4094) |
How do you unistall STEP 7 (TIA Portal) completely? You uninstall STEP 7 (TIA Portal) completely via MS Windows functions or via the Inventory Tool (STEP 7 (TIA Portal) V13+SP1 and higher). Description 1. General uninstallation of all TIA Portal versions via the Control Panel or using the STEP 7 (TIA Portal) CD: a. In the Control Panel you open the "Change/Remove Programs" dialog and double-click the "Siemens Totally Integrated Automation Portal Vxx" application. Acknowledge the message that follows with "Yes" and follow the instructions on the screen. b. Alternatively you can also do the uninstallation using the STEP 7 (TIA Portal) CD. Insert the CD in the CD drive of your computer and open the "Start.exe" file. Select the dialog language and then enable the "Uninstall" option field and follow the instructions on the screen. |
This contribution was helpful to2 thankful Users |
12/30/2020 5:00 PM | |
Posts: 18 Rating: (5) |
Thanks! The DVD did the job. Windows did not work with uninstaller. |
This contribution was helpful to1 thankful Users |
Follow us on