1/11/2023 10:55 AM | |
Joined: 12/23/2021 Last visit: 2/21/2024 Posts: 234 Rating: (23) |
Hi! You probably find useful the following FAQ from the Siemens official web: How do you create dynamic text lists in WinCC (TIA Portal)? In the following link to the TIA Portal Professional V17 manual you can find more information on how to work with text list that may also help you: |
If this post helped you in any way, please rate it positively. |
|
1/17/2023 12:49 PM | |
Joined: 8/3/2009 Last visit: 4/23/2024 Posts: 12834 Rating: (1639)
|
Hello Sergey_78 you could use a combobox object in your screen. at the screen open event you can rund an initial script to fill the entries. If a value or a text changes you can also use a script on the object itselfe with tag triggers to update the entries. something like this LINK A dynamic entry like in WinCC Comfort/Advanced is not possible with textlists. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on