7/22/2021 11:40 AM | |
Joined: 5/18/2020 Last visit: 9/9/2024 Posts: 15 Rating: (0) |
I'm trying to do this but also running into problems. I'd like to email the .CSV data log on a weekly basis. it seems not possible using winCC or VBS? Windows task scheduler no longer supports this. I wrote a powershell script as above it does not seem to work as it reports the logging file is in use. Also is it better to call this from the HMI using VBS (example please?) or to use the task scheduler if running a windows HMI? There's a lot of people trying to do this on here and it seems a fairly obvious desirable feature. So I think it should be a feature of TIA to send attachments or an additional thread on here for people to post a solution that works. THanks Rich ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/22/2021 12:50:05New subject after splitting |
|
7/22/2021 4:45 PM | |
Joined: 10/10/2014 Last visit: 8/28/2024 Posts: 1725 Rating: (210) |
Hi GrennFlach, I the follow FAQ you can find an examples for emails Toolbox for HMI Projects https://support.industry.siemens.com/cs/de/en/view/106226404 Best regards schufri |
1/18/2023 4:19 AM | |
Joined: 2/6/2020 Last visit: 9/20/2024 Posts: 1 Rating: (0) |
Hi, can you share details with examples. |
1/18/2023 11:57 AM | |
Joined: 8/3/2017 Last visit: 6/11/2024 Posts: 1086 Rating: (53) |
Hi Sudhir, please read the posted FAQ and then ask precise questions to be able to get good answers.
|
Please, check out the forum search to find already existing topics regarding your issue and to get some hints. |
|
Follow us on