1/27/2023 4:22 PM | |
Joined: 1/26/2023 Last visit: 1/27/2023 Posts: 1 Rating: (0) |
J’ai un PC 670 sous Windows NT 4.0 SP5 avec WinCC V4.0.1.3 qui est hors service. N’ayant plus le CD d’installation de WinCC V4.0.1.3, nous souhaiterions faire une migration vers une version plus récente V7 avec un IPC. Voilà lors de la migration vers la version V5.0 SP2, le protocole de communication n’apparaît pas avec les variables. Est il possible que vous m’assistez à faire la migration, il vous plaîtM. BEAN1 ------------------------------------------------------------------------------------------ AttachmentMIGRATION WINCC V4 vers WINCC V5.0 SP2.pdf (170 Downloads) |
Last edited by: Jen_Moderator at: 02/08/2023 11:15:05New subject after splitting |
|
1/30/2023 9:58 AM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1641)
|
Hello Mr BEAN1 Please write your answers in english because this is an english forum. Here your Text from translator: " I have a 670 PC running Windows NT 4.0 SP5 with WinCC V4.0.1.3 which is down. As we no longer have the WinCC V4.0.1.3 installation CD, we would like to migrate to a more recent version V7 with an IPC. So when migrating to version V5.0 SP2, the communication for general migration help have a look at this: https://support.industry.siemens.com/cs/ww/en/view/44029132 |
Last edited by: Murof at: 01/30/2023 09:59:08If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on