2/2/2023 8:09 AM | |
Joined: 8/3/2009 Last visit: 4/18/2024 Posts: 12813 Rating: (1633)
|
Hello nestor-dejuan First check the steps in the basic FAQ: https://support.industry.siemens.com/cs/ww/en/view/58522603 then check this one, perhaps the transfer mode on the panels have changed: https://support.industry.siemens.com/cs/ww/en/view/88633853 Then check also that you are completley offline to any plcs before loading the HMI. and use also the dropdown list with "Devices with same IP Adresses" (not the compatible devices option) perhaps something is blocked or you came from a different subnet... If nothing helps you can also use the offline transfer: https://support.industry.siemens.com/cs/de/en/view/109740696 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on