2/5/2023 4:50 AM | |
Joined: 8/19/2017 Last visit: 4/28/2024 Posts: 79 Rating: (3) |
Dear User Welcome to the Process Automation! First of all I recommend you to start with PCS7 Compendium as the starting manual. It is updated and includes all necessary information about PCS 7. For your problem about converting charts to the blocks, I don't really understand why you try to convert a chart that contain for example valve block to a block? The main idea of the DCS is to use simple and common blocks in library that includes faceplates to connect with HMI for monitoring and controlling the process. When you use a valve block inside a chart that compiled as a block, you loose all HMI capability of the block. For common ways of using PCS 7 and blocks, This is a demo project of PCS 7 that you can see what are the common ways of configuring project and using blocks. It used CEMAT library but the idea is the same. Best regards. |
Last edited by: Soroosh.v at: 02/05/2023 05:04:29 |
|
Follow us on