2/7/2023 1:58 PM | |
Joined: 9/4/2020 Last visit: 4/27/2024 Posts: 6 Rating: (0) |
Hello, I am using PCS7 V9.1. I have one small problem regarding local mode operation of MotL block. I don't have local-remote feedback IO but Ihave to show if motor is running locally. So Ihave written logic as if start commnad is not present and Run feedback is present then LocalLi = 1 and StartLocal = 1. But I don't want my Start Output to be get affected while in local mode. Is tgere any solution on these????? ------------------------------------------------------------------------------------------ |
Last edited by: Charudatta at: 02/07/2023 14:03:23Last edited by: Jen_Moderator at: 02/08/2023 07:20:25New subject after splitting |
|
Follow us on