2/16/2023 11:30 AM | |
Joined: 7/19/2022 Last visit: 7/30/2024 Posts: 378 Rating:
|
Hello Learning_Fast, The code blocks and program data are located in working memory. While blocks and configuration not relevant to the program execution are stored in the load memory. I attach a FAQ that I recommend you to have a look at: Differing information on the requirement of offline/ online memory In addition, the S7-300 manual also explains each memory area: SIMATIC S7-300 CPU memory areas
|
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to
1 thankful Users |
Follow us on