3/14/2023 6:24 PM | |
Joined: 8/5/2019 Last visit: 4/17/2024 Posts: 6 Rating: (0) |
Hi to all, I am developing a machine using the PackML standard for the first time. Searching the various application example on the Siemens website, the best solution that I have chosen is the Machine Template example, a very well done job which provide a clear implementation,documentation and example for start the developing of your machine. In my case, the machine is divided in two EM: EM01 which have one TM and one CM, and EM02 which have one EM and two CM. Starting the develop from the CM and going up, I am now stuck on the state machine communication between the two EM. In the machine template documentation I found the following FB: (attached image), which in my opinion don't provide a complete communication example between two or more EM. My machine will start to work with the EM01 and after that the Execute status of the EM01 is end (so is in the Complete status) the EM02 need to start to work too. My question is: how to implement the clearly and correctly possible the state machine communication between two or more EM? Maybe I am using the wrong FB for my purpose.. I hope that somebody can help me with any suggestion Thanks a lot in advance to all! |
Last edited by: l.carminati at: 03/14/2023 18:26:27Last edited by: Jen_Moderator at: 03/15/2023 08:34:28Link optimized. Text formatting optimized. |
|
Follow us on