12/8/2022 7:01 AM | |
Joined: 5/7/2021 Last visit: 12/23/2022 Posts: 3 Rating:
|
Hello everyone, I have a project to connect S7-1500 OPC UA Client (simulate with PLCSIM Adv) with OPC UA Server (build in .NET) on VPS. When I use Prosys Client to connect with server on VPS, it works normal. But when I change to S7-1500 client, the OPC_UA_Connect status is 0070_0200 and Busy is TRUE. A while later, the status change to 0070_0000 and notthing happen. No ConnectionHdl and for sure, my server on VPS does not receive anything. I connect with no security. I can connect to Server with the Client_interface but the OPC_UA_Connect still not work. Has anyone can help me with my problem? Thanks for all your help. Attachmentattachments.zip (240 Downloads) |
12/13/2022 9:58 AM | |
Joined: 8/3/2009 Last visit: 6/26/2024 Posts: 13122 Rating:
|
Hello 131hvcuong check also the basic example, perhaps it helps: https://support.industry.siemens.com/cs/de/en/view/109762770 bye Murof |
If this Information really helps, you could use the Rate function |
|
3/28/2023 9:55 AM | |
Joined: 3/28/2023 Last visit: 3/29/2023 Posts: 1 Rating:
|
The thread's a bit old but I still won't do ask whether you have checked your firewall settings on the VPS? It's possible that the S7-1500 client is being blocked by the firewall, which could be causing the issue. Also, have you tried connecting to the OPC UA server with any other clients besides Prosys? It could help narrow down if the issue is with the S7-1500 client specifically or if there's something else going on. Also, have you considered using a dedicated server instead? Dedicated servers like the ones from ishosting.com/en/dedicated can offer more control and better performance for certain types of applications |
Last edited by: fatatris at: 03/29/2023 13:58:51 |
|
Follow us on