3/30/2023 5:03 PM | |
Joined: 6/11/2019 Last visit: 7/13/2024 Posts: 2205 Rating:
|
If I understood you correctly, you need a continuous pulse generator that switches 4 channels one after the other. This is interrupted when a bell signal is requested. Only when this has been processed is the pulse generator continued (see appendix). Of course, you can also do this with a step chain. In both cases, however, the order of the outgoing signals is fixed. However, if you want to take the order into account, then it gets really complicated. By the way, welcome to the forum. greeting Ella_68 Attachment4 Bell.zip (399 Downloads) |
Follow us on