4/20/2023 2:42 PM | |
Joined: 5/30/2022 Last visit: 4/26/2024 Posts: 520 Rating: (85) |
Hi Hunterseeker1, We can only speculate on how CPUs would behave if the ambient conditions in the technical specifications are not observed:
With a relatively high probability, the CPU is not noticeable in the limit range, but we are formally outside the guaranteed environmental conditions and cannot make any statement about the behavior. Ambient temperature and installation altitude |
If this information really helps, you could use the Rate function. |
|
Follow us on