4/23/2023 12:32 PM | |
Joined: 2/2/2016 Last visit: 5/29/2024 Posts: 1 Rating:
|
After print from Graphics pages, Trend views or LogViwer to pdf, created pdf file is always blank. Any idea ? Thankx
|
4/24/2023 5:21 AM | |
Joined: 6/4/2010 Last visit: 7/5/2024 Posts: 381 Rating:
|
Dear Dusan, This looks to be the well-known Microsoft issue and the same as: https://support.industry.siemens.com/forum/ww/en/posts/desigocc-not-printing-chart/293275 This issue was related to a specific Microsoft update. Please read the Microsoft kb5022083 for detailed information. See: Imporant part is: “Resolution This issue was addressed in out-of-band updates released January 31, 2023, for Windows 10, version 1607 and Windows Server 2016 versions and newer operating systems and out-of-band updates released February 17, 2023 for earlier Windows and Windows Server versions. To get the standalone package for these out-of-band updates, search for the KB number in the Microsoft Update Catalog. You can manually import these updates into Windows Server Update Services (WSUS) and Microsoft Endpoint Configuration Manager. For WSUS instructions, see WSUS and the Catalog Site. For Configuration Manger instructions, see Import updates from the Microsoft Update Catalog. If you used any workaround or mitigations for this issue, they are no longer needed, and we recommend you remove them. To remove workaround review the workaround or alternative workaround which was applied for instructions.” Best regards, Albis |
Follow us on