5/5/2023 4:44 AM | |
Joined: 3/30/2020 Last visit: 7/19/2024 Posts: 4631 Rating:
|
These notes are in compliment the response from Mr. Madadi. Anything our volunteers say will be guessing until you study the documentation of the pump. There is a very good chance that Modbus RTU protocol over RS232 is used, for example. Then the instructions you think you need is in actual fact not what you need. Consider also looking at the in-software help on how to use the instructions you identified. Use the search facility in the forum to get old topic or some application example from the knowledgebase. The spoon-feeding process robs time and invites frustration. An article that already could be helpful if ASCII is used .. As a general forum usage hint - the volunteers who help out on this forum are more likely to spend invest time on a topic where the topic starter is putting effort into his own problem. I cannot see that you are trying very hard to work. Please prove me wrong. |
Last edited by: qwazee at: 05/05/2023 04:45:23Last edited by: qwazee at: 05/05/2023 04:49:44Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
3 thankful Users |
Follow us on