5/14/2023 6:40 AM | |
Joined: 4/6/2021 Last visit: 7/25/2024 Posts: 21 Rating:
|
We need to tune 6RA80 Drive for 3 KW DC motor , Maximum arm voltage is 220V Drive Details : 6RA8018-6fv62-0aa0, rated voltage of drive Motor Details : Rating : 3KW, Speed : 400/2000 rpm, Rated Arm Voltage : 220V Rated Arm Current 3.5/18A Rated Field Current: 2.38A at 175 Volt, 400 rpm Minimum filed 0.23A at 18V, 2000 Rpm Encoder details are as given below. POG86E TN1 DN 1024 I, supply : 9 to 30 v dc HTL we given 400 V as supply to motor, speed tuning not completing. Armature tuning completed, but while checking base speed of the drive delivering 80volt maximum at speed reference 100% speed refence. As per our local agency support, they suggested to give 220V , 3Phase as incoming supply to drive then tuning part will complete properly. Please confirm is it necessary to do it or any other option required. new drive parameter at as attached Attachment6RA80-TABLE DRIVE.zip (265 Downloads) |
Follow us on