5/20/2023 1:56 AM | |
Joined: 5/18/2023 Last visit: 5/20/2023 Posts: 4 Rating:
|
Hi, I'm facing a similar issue and I'm unsure about the appropriate course of action. Here's my situation: I'm using WinCC V7.5 with Webclients. Over the past two days, I made several modifications, such as adding new connections, pictures, and a few OnlineTableControls. When I review these changes on the Server Runtime, everything seems to be working fine. However, when I stopped the Runtime to publish the changes using the Publishing Wizard, I encountered an error. Upon checking the WizardLog.txt, I noticed that the same error appears for every PDL (Process Display Language) that I edited or created in the last two days. The error message remains the same, only with a different PDL name each time. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/22/2023 11:31:06New subject after splitting. |
|
5/22/2023 12:11 PM | |
Joined: 5/6/2022 Last visit: 7/5/2024 Posts: 429 Rating:
|
Hi Liamcarter, Could you offer us some more information about the error you mention? Could you share some screenshot about the error message you get? Additionally, what exact wincc version do you have? What OS versions do you have? Do you have correctly configured client-server? Best regards! |
If this Information really helps, you could use the Rate function |
|
5/22/2023 12:39 PM | |
Joined: 8/11/2021 Last visit: 7/4/2024 Posts: 9 Rating:
|
Hi, Try to install the last WinCC Update as well. |
5/23/2023 1:47 PM | |
Joined: 8/3/2009 Last visit: 7/11/2024 Posts: 13283 Rating:
|
Hello Liamcarter you can try to clear the dcf file: https://support.industry.siemens.com/cs/de/en/view/109763043 And also clear the content of the webnavigator folder in your project directory (close the WinCC project and editor before and do a backup befor testing this) After this open the project again and do the publishing again. If there was an inconsitency in the webfiles then it should be gone. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on