Industry Online Support
Technical Forum
5/8/2023 9:30 AM | |
Joined: 2/29/2008 Last visit: 6/25/2024 Posts: 8 Rating:
|
I have a Simatic IOT2040 and configured it it as per given procedure in manual. Now I am trying to load the RT IOT2040 PN Driver using WinSCP but I found there is mismatch in path shown in manual. Image on SD card is not matching and so showing error while loading the driver in IOT2040 device. For more information I have attached a screen shots, pls refer it and provide the proper image file or RT IOT2040 PN Driver. Following files are used for configuration 1. IOT2040_Example_Image_V3.1.17.zip 2. RT__IOT2040_PN_Driver_V2.4.0.zip 3. RT__IOT2040_PN_Driver_Quick_Start.pdf AttachmentSR_Screenshots.zip (381 Downloads) |
6/1/2023 9:56 AM | |
Joined: 4/28/2015 Last visit: 6/3/2024 Posts: 3345 Rating:
|
Hi, for using the PNDriver you need to use the RT_Image_V2.4 from here. (IOT2040_RT_Example_Image_V2.4.0.zip (365,0 MB) Best regards! |
Last edited by: bergmanu at: 06/01/2023 09:56:49Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on