6/12/2023 3:07 PM | |
Joined: 10/22/2020 Last visit: 5/17/2024 Posts: 169 Rating: (6)
|
Hello donlewis, please take a look at the IOT2050 Operating Insructions. Regarding NodeRED, please try the preinstalled mraa-gpio-ain Node. Keep in mind to use the terminal command iot2050setup to access the settings of the IOT2050. Navigate to the GPIO settings under the menu option Configure Arduino I/O. BR |
This contribution was helpful to1 thankful Users |
6/15/2023 3:43 PM | |
Joined: 6/12/2023 Last visit: 6/22/2023 Posts: 2 Rating: (0) |
Thanks, but there are additional i/o that is not on the i/o shield. How do I access those? |
6/27/2023 11:08 AM | |
Joined: 10/22/2020 Last visit: 5/17/2024 Posts: 169 Rating: (6)
|
Hello donlewis, are we talking about the bare GPIO's on the IOT2050 or the I/O Module Shield (additional Hardware)? BR |
Follow us on