6/9/2019 10:04 PM | |
Posts: 25 Rating:
|
Dear All, Its first time to me to buy PC adapter USB A2 USB adapter to program PLC I find this one in Siemens Industry mall 6GK1571-0BA00-0AA0 PC adapter USB A2 USB adapter (USB V2.0) for connection of a PG/PC or notebook to SIMATIC S7 via PROFIBUS or MPI contain USB cable 5 m, MPI cable 0.3 m can be used under Windows XP/Vista/ Windows 7 32/64-bit and higher I just want to ensure that it works with Win 10 Thanks in advance |
6/9/2019 10:44 PM | |
Joined: 9/27/2006 Last visit: 7/11/2024 Posts: 12268 Rating:
|
Hello; The best source for this type of information is the manual: SIMATIC PG/PC - PROFIBUS PC Adapter USB A2 Operating Instructions https://support.industry.siemens.com/cs/us/en/view/68849363 So: The PC Adapter USB A2 is compatible with Windows 10, as long as you have installed a programming software that is compatible with Windows 10 (check the supported version), such as Step 7 v5.6, https://support.industry.siemens.com/cs/us/en/view/109747706 or Step 7 Professional v15: https://support.industry.siemens.com/cs/us/en/view/109752225 Hope this helps, |
6/10/2019 6:34 AM | |
Posts: 25 Rating:
|
Thank you sir |
8/7/2023 4:26 AM | |
Joined: 7/31/2023 Last visit: 8/7/2023 Posts: 1 Rating:
|
I can't install simatic pc adaptor usb a2 on window 10. |
Follow us on