8/9/2023 10:52 AM | |
Joined: 8/7/2023 Last visit: 5/15/2024 Posts: 2 Rating: (0) |
Hi. Please tell me how to quickly close and open the block interface panel (the place where you declare a local variable), except with the mouse.? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/09/2023 11:15:51New subject after splitting |
|
8/9/2023 2:24 PM | |
Joined: 7/7/2010 Last visit: 5/17/2024 Posts: 14751 Rating: (2370)
|
In the horizontal line between the interface and code panels you should see an arrow at the midpoint of that horizontal line. Click it. Click-n-drag the line itself to grow or shrink the interface panel height. Once you like the default interface panel and main window size and relationship, click the window setting save button so portal remembers how you like that block to open in the future.
|
science guy |
|
8/10/2023 6:54 AM | |
Joined: 8/7/2023 Last visit: 5/15/2024 Posts: 2 Rating: (0) |
Dear Einstein, you misunderstood my question. I know how to close this window and where to click with the mouse. But I asked how to close this window WITHOUT USING THE MOUSE. Do you know what keyboard shortcuts, such as ctrl+... so that you can quickly close this window or open it??? I know that if you point to the tag in the code text and press CTRL+Shift+D, it will move to the area I highlighted in red. If you press CTRL+Shift+G, it will move back to the tag in the code area. But this method does not always work. Anyway, thanks for answering my question, I didn't expect such a quick reaction))
|
Follow us on