6/1/2009 10:36 PM | |
Posts: 95 Rating: (0) |
Hello I am trying to configure routing so I can connect to a MM440 with starter. I found the following FAQ http://support.automation.siemens.com/US/view/en/23432199 but the connection is different (drive on ethernet, PG on Profibus). In my case, I have a drive on Profibus and PG on ethernet. This is a small demo case application. The S7-300 cpu is a 313c(313-6cf03-0ab0 v2.0)with an 343-it(343-1gx20-0xe0 v1.0)module. All are listed in the tables as capable of routing. The drive is on the profibus network of the CPU. I tried to follow the PDF and swap the profibus and ethernet, but no luck. I get through the netpro and have the highlighted yellow line, but when I start the starter software, I get no connection. The PG interface is set to tcp/ip. Is there a more definitive document to describe routing? regards john |
6/2/2009 7:48 AM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello, Look at What should I do if I have set my PG/PC interface to ISO-Industrial Ethernet so I can use Routing with Starter and DriveES to access MICROMASTERS on Profibus from the network port on my PG or PC and I find that the communication doesn't work? Perhaps would be useful. Best regards Hristo Mihalev |
6/3/2009 4:54 PM | |
Joined: 5/12/2006 Last visit: 6/4/2024 Posts: 22254 Rating: (2986) |
hello, please can you post a screenshot of the errormessage? Regards Christoph |
6/4/2009 2:45 PM | |
Posts: 95 Rating: (0) |
thanks guys, I posted another thread on this subject when I couldn't find this one not realizing the moderator moved it. Please refer to the other threadrouting PG on profinet and MM440 on Profibus as it is more active with responses. john |
Last edited by: CS Moderator at: 6/5/2009 9:59 AMlink to other thread added. and thread closed |
|
Follow us on