9/20/2023 12:04 PM | |
Joined: 4/18/2023 Last visit: 2/27/2024 Posts: 4 Rating: (0) |
Ok, here are the 300 and 1500 configurations. The 300 shows the part number and firmware version, the PN interface has been selected and the I-Device enabled, along with an I and O area defined. The GSD file was created using Options, Create GSD file for I-Device.. in the HW Config. The 1500 shows the part number and firmware version and the attempted import of the GSD file, it is selected but the Install button is grey out. Thanks. AttachmentConfig.zip (131 Downloads) |
Follow us on