9/26/2023 8:06 AM | |
Joined: 9/4/2023 Last visit: 4/9/2024 Posts: 4 Rating: (0) |
greetings, I am the intern taking over from radusti333 and have added the following lines to the extra defconfig but am still unable to load either the peak_pci or the mcp251x driver. the peak_usb driver works fine however so no clue as to what is goingg wrong here. CONFIG_CAN_PEAK_PCIEFD=y thx for the help in advance Max van Eck ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/27/2023 11:24:26New subject after splitting |
|
9/27/2023 11:25 AM | |
Joined: 6/19/2017 Last visit: 6/7/2024 Posts: 8154 Rating: (165) |
Closed cause question posted twice. The second thread with the subject Unable to load either the peak_pci or the mcp251x driver is published within the conference IOT2050. Best regards, |
My Forum is the place to personalize your profile, |
|
Follow us on