10/10/2023 1:54 PM | |
Joined: 2/17/2020 Last visit: 6/21/2024 Posts: 1014 Rating:
|
Hi, Is Step7 OEM version listed in Windows Control Panel - Programs and Features? If so uninstall that. There are some Siemens software that install just the framework of the Simatic Manager, that is referred to as "Step7 OEM" version. Commonly its’ "Starter ". If one of those software is installed and one tries to install Step7 5.x, get the issue that you encountered. To install Step7 5.x: 1) the software that has installed OEM version, in this case Starter 5.X' must be uninstalled, via windows control panel 2) also via control panel remove Step7 OEM version 3) install Step7 5.x , and then 4) re-install the software that was uninstalled at item 1). Please see: Point 3. How can you install STEP 7 if a version of STEP 7 OEM is already installed on the PC? |
A rating will be well appreciated. |
|
Follow us on