10/18/2023 3:56 PM | |
Joined: 10/18/2023 Last visit: 10/20/2023 Posts: 1 Rating: (0) |
I'm working with an IoT2050 FS:05 device; when I try to modify a file, it tells me that there's no more storage space available. Checking the size of the files I found that the auth.log file located in directory /var/log is very large and contains lots of logs stored every second. The file was emptied and the behavior still the same; analyzing the content of the logs most of them indicate access to the /etc/mel-os/cache folder as attempting to manipulate the contained files using the gdbmtool and other many logs. I have been looking for a way to disable log storage, without success. Is there any way I can disable the logs to prevent the file growing? I attach a fragment of the file with some logs that are generated.
Attachmentauth.zip (267 Downloads) |
Follow us on