10/17/2023 2:42 AM | |
Joined: 10/2/2023 Last visit: 4/30/2024 Posts: 1 Rating: (0) |
Im using a Simatic 400H system and trying to set up IEC104 communication. I added the "CD_SIPLUS_RIC_IEConS7-400_V1_7_1" library and also copied all blocks from the sample to my project. I also made a CFC that contains FbDiln to generate OB during compilation. Cannot compile/download CFC because of the above error. When I remove the FB106 block, the error would be "No Element Found". When I try to download the H station in simatic manager, prompt that im unable to copy blocks. The funny thing is when I remove the block and go online, the block reappears again. I have attached some picture and the diagnostic buffer for your referal, would appreciate any help given -Sheep AttachmentCPU410E Diagnostic Buffer v3.pdf (381 Downloads) |
Last edited by: AutoGen_7271415 at: 10/17/2023 02:45:15 |
|
Follow us on