10/18/2023 2:10 PM | |
Joined: 5/13/2022 Last visit: 6/27/2024 Posts: 5 Rating: (0) |
Hi i have a question with most likely a simple awnser ;) in a old programm i have used a analog mux where i could choose the referens block to use it value with a new program i build it is gone, (see attachment) moste likely it has something to do that the new program is a network of 5 logo's and the old one wasnt . can somone put me on the right track? thank Attachmentlogo.pdf (305 Downloads) |
10/18/2023 4:40 PM | |
Joined: 12/18/2014 Last visit: 7/1/2024 Posts: 33265 Rating: (4116)
|
The PDF file is absolutely not helpful. Please upload the your programs (old and new) as a ZIP file to the forum. |
10/18/2023 5:13 PM | |
Joined: 12/18/2014 Last visit: 7/1/2024 Posts: 33265 Rating: (4116)
|
Or this link: How can you configure references between blocks in LOGO! 8? |
This contribution was helpful to2 thankful Users |
10/20/2023 5:44 AM | |
Joined: 5/13/2022 Last visit: 6/27/2024 Posts: 5 Rating: (0) |
thanks that was the awnser i was looking for just never needed/used it. works fine now |
Follow us on