10/26/2023 7:07 AM | |
Joined: 3/11/2019 Last visit: 7/5/2024 Posts: 1505 Rating: (270) |
Hi,
That is basically the correct procedure. If you need a snapshot depends mostly on your requirements/machine... it's not a must have. SIMATIC STEP 7 Basic/Professional V18 und SIMATIC WinCC V18The backup includes all data that are needed to restore a particular configuration version of a CPU. The following data is backed up, for example:
The backup is performed with the current values of the CPU. Entries in the diagnostics buffer are not included in the backup, and neither is the current time. The backup does not contain the password to protect confidential PLC configuration data. regards sancruz |
Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
Follow us on