11/6/2023 2:08 PM | |
Joined: 11/6/2023 Last visit: 11/6/2023 Posts: 3 Rating: (0) |
So looking at other threads i noticed there are 3 generations of the logo. Is there a table/link that shows the various model #s and their related generation? or could someone fill in the ?s for me? 08A8- 8.0 (1st) 08A7 -? 08A6 -? 08A5 -? 08A4 -? 08A3 -? 08A2 -? 0BA1 -? 0BA0 - 8.2 (3rd) BTW, i did see this for the 8.2 model #s so that was very nice |
Last edited by: Jen_Moderator at: 11/07/2023 07:55:17Link optimized. |
|
11/6/2023 3:29 PM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32895 Rating: (4066)
|
In the linked topic it goes of the 3. generation of 0BA8 LOGO!s. The current LOGO! 8.3 is the 4. generation of 0BA8. See attached text file. The next LOGO! that will come is a LOGO! 8.4 AttachmentVersions of 0BA8.txt (276 Downloads) |
This contribution was helpful to1 thankful Users |
11/6/2023 4:48 PM | |
Joined: 11/6/2023 Last visit: 11/6/2023 Posts: 3 Rating: (0) |
Thank you for the answer |
This contribution was helpful to1 thankful Users |
Follow us on