7/5/2016 9:01 AM | |
Posts: 18 Rating: (2) |
I am using CPU315-2 PN/DP and SIMATIC RF180C(6GT2002-0JD00) with 6GT2002-1JD00.I want to do the programming in simatic manager.I am not getting the gsd file of SIMATIC RF180C(6GT2002-0JD00).All the links from siemens site example is mention the TIA PORTAL v13.Is it possible to configure in simatic manager?while i trying to download the gsd from siemens site below link,the download get failed.Plese give some suggestions or links for the gsd file of SIMATIC RF180C(6GT2002-0JD00) .Is there any separate license needed for the gsd/fb45 block? https://support.industry.siemens.com/cs/document/22747865/profinet-gsd-files%3A-identity?dti=0&lc=en-WW ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 7/6/2016 11:40:18 AMNew subject after splitting |
|
7/6/2016 1:51 PM | |
Posts: 18 Rating: (2) |
I am able to download all the other gsd file in that page,But when i am trying to download the below link the gsd "file not found" is showing in page.Also please give the link or suggestion to download the fb45 block. Station type:RF180C |
This contribution was helpful to1 thankful Users |
7/7/2016 10:43 AM | |
Joined: 10/1/2013 Last visit: 5/8/2024 Posts: 605 Rating: (71)
|
This is strange, I was klicking on the link in your post and it worked for me. I'm afraid there is no download anymore for FB45. You need to organize the SIMATIC RF DVD. e:/ Alternatively you could use the block "Ident_Profile" to operate your RF readers via RF180C: |
Last edited by: Owei at: 7/7/2016 10:44:34 AM |
|
This contribution was helpful to1 thankful Users |
11/12/2023 2:57 AM | |
Joined: 3/16/2022 Last visit: 8/26/2024 Posts: 1 Rating: (0) |
我也没有找到 |
7/31/2024 3:35 PM | |
Joined: 7/7/2024 Last visit: 8/6/2024 Posts: 1 Rating: (0) |
Attachmentgsdml-v2.zip (205 Downloads) |
Follow us on