Industry Online Support
Technical Forum
11/26/2023 3:41 PM | |
Joined: 11/15/2023 Last visit: 11/26/2023 Posts: 4 Rating:
|
Hello, I have a system with a LOGO! 8 and the TP400 keyless. I want to press a button and send this as a boolean to the LOGO! (i.e. send a boolean "1"). This will be activated untill a certain hour is passed (e.g. 21:00). After that, I want the LOGO! to switch off the button on the HMI (i.e. send a boolean "0"). That way, the operator can see that a machine is not turned on anymore. The problem I have is that the HMI turns on the button and the LOGO! sees that. After that time the LOGO! sends out a "0" to the HMI. But in the LOGO!, the network input is still high. The network input doesn't turn off, eventhough the network output of the LOGO! is off. I really hope someone can point me in the right direction. Thank you in advance.
AttachmentMachinefabriek_met_beeldscherm.zip (274 Downloads) |
11/26/2023 4:17 PM | |
Joined: 11/15/2023 Last visit: 11/26/2023 Posts: 4 Rating:
|
I made some screenshots. Please say if you need another screenshot: |
11/26/2023 6:09 PM | |
Joined: 12/18/2014 Last visit: 7/18/2024 Posts: 33374 Rating:
|
Maybe this can help you.
AttachmentMachinefabriek_V2.zip (255 Downloads) |
Follow us on