11/23/2023 12:47 PM | |
Joined: 5/30/2022 Last visit: 4/29/2024 Posts: 520 Rating: (85) |
Hi Baskaran1405, I have never seen those types of requirements to log in on an HMI panel haha, but you will have to do it by scripting, I don't know if it will be possible, since the scripting possibilities are limited in a Comfort Panel, there are many more possibilities in a Unified panel for example, the only thing I can think of is to attach the scripting manual: SIMATIC HMI WinCC (TIA Portal) WinCC Engineering V17 – Programming reference But I understand that other security methods would be more appropriate, such as using an RFID card: |
If this information really helps, you could use the Rate function. |
|
This contribution was helpful to1 thankful Users |
Follow us on