12/6/2023 3:25 PM | |
Joined: 3/14/2008 Last visit: 8/3/2024 Posts: 2079 Rating: (931)
|
Hi, A license must be installed on the CPU410 Expansion Card in order to run with a PROFINET Redundant network. But I can save you that money! Since firmware V8.2.4 of the CPU410-5H, the redundant license is not checked anymore. This means you can run redundant networks without license. You need to upgrade to V8.2.4. For reference the license is available with the following MLFB: 6ES7653-2CX01-0XE0 SIMATIC PCS 7, software, CPU 410 Expansion Pack (PN red) required to utilize redundant PROFINET subnets Upgrade Option for 1 installation (1 x AS, 2 x CPU) R-SW, without SW, without documentation License Key on USB stick Class A, for more information, see PCS 7 V9.0 Readme Reference HW: PCS 7 IPC Bundle ******************************* Content: 1x USB |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
12/8/2023 6:07 AM | |
Joined: 2/29/2016 Last visit: 3/12/2024 Posts: 100 Rating: (1) |
Wow! Thank you for this valuable information! |
12/8/2023 9:18 AM | |
Joined: 3/14/2008 Last visit: 8/3/2024 Posts: 2079 Rating: (931)
|
Hi, You can select just a file and the article number of the CPU410 is shown. Does not matter which one. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on