12/13/2023 2:59 PM | |
Joined: 5/30/2022 Last visit: 4/26/2024 Posts: 520 Rating: (85) |
Hi Pandiani, The build you have indicated is Windows Pro 22H2, so there are no compatibility problems, in the forum we can not help you, so I recommend you to open a Support Request for Siemens to evaluate the log and the project. AttachmentMicrosoft-Windows-10_es_2023-12-13.xlsx (164 Downloads) |
If this information really helps, you could use the Rate function. |
|
This contribution was helpful to1 thankful Users |
12/13/2023 3:37 PM | |
Joined: 10/31/2005 Last visit: 4/22/2024 Posts: 340 Rating: (31) |
Thank you, I'll open the request, just as I suspected I'd have to. Thanks for the help! |
Follow us on