12/13/2023 3:21 PM | |
Joined: 5/6/2022 Last visit: 8/13/2024 Posts: 439 Rating: (86) |
Hi JFKSC, In this case I would recommend an UPGRESS of the Firmware of the PLC and the display to its most current versions. Next, I share the link where you will find the most up -to -date versions of the PLC: "FIRMWARE UPDATE FOR CPU 1518F-4 PN/DP" Try to update it and see if you continue with the same behavior. If so, it would be good for us to eat the diagnostic buffer in .Txt to see if it can give us more imformation. Best regards! |
If this Information really helps, you could use the Rate function |
|
12/13/2023 4:54 PM | |
Joined: 5/31/2023 Last visit: 6/19/2024 Posts: 2 Rating: (0) |
Thanks. I will try soon possible. |
Follow us on