4/28/2022 7:27 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi Cristian, the answer is very simple. You can't configure the OS Clients, because you don't have to do it. Every OS Server generates his own server packages. This server package has all the information for the OS Clients, that the OS Client needs to operate with the OS Server, like the IP address. If you are setting up a completely new PCS 7 project, I can recommend you the manual PCS 7 Compendium Part A - Configuration Guideline that includes a step for step instruction to set up a PCS 7 project. With regards |
4/29/2022 5:19 AM | |
Joined: 2/22/2021 Last visit: 3/24/2024 Posts: 114 Rating: (12) |
|
Last edited by: cristian021091 at: 04/29/2022 05:20:55 |
|
4/29/2022 5:20 AM | |
Joined: 2/22/2021 Last visit: 3/24/2024 Posts: 114 Rating: (12) |
Thank you so much, your support was very helpfull
|
Last edited by: cristian021091 at: 04/29/2022 05:21:10 |
|
This contribution was helpful to1 thankful Users |
12/15/2023 11:57 AM | |
Joined: 8/21/2014 Last visit: 4/26/2024 Posts: 949 Rating: (13) |
New question published by AutoGen_6615511 is split to a separate thread with the subject The Target PC is not accessible error. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on