8/19/2014 1:42 PM | |
Joined: 10/28/2008 Last visit: 7/21/2023 Posts: 245 Rating:
|
HiSachinpatke. Thank you for answer. I found also this information inArets link.. Now it seems that I can find all information I need. I tried to use "SZL_ID:W#16#B1", but index of this SZL_ID is "Logical base address" from HW. I do not have address for CPU in HW configuration for whole CPU, only for ports "MPI/DP", "PNIO", "Port1" and "Port2". So I am using now"SZL_ID:W#16#B1", where index is "Rack, slot". Firstly I want to read CPU diagnostics via"SZL_ID:W#16#B1" and rack=0, slot=2. But for now I have in Ret_Val "error 8085: Due to a problem in the system, information is not currently available (for example, dueto a lack of resources)." I tried to set different parameter in HW config of the CPU, tried to restart the PLC etc., still without success, PLC is in RUN and there is no SF on it, diagnostic buffer is empty... So I will solve this problem and then I will continue |
Georgio |
|
Follow us on