9/27/2022 12:19 PM | |
Joined: 3/11/2019 Last visit: 8/14/2024 Posts: 1555 Rating:
|
Hi EloyJSB, as already mentoined earlier in this post, this was fixed with update 2 for V17 (in the meantime update 5 is available). It is not necessary to deactivate the service/protocol. Just install the latest update. If STEP 7 classic V5.7 is installed in parallel on the same system, also install latest hotfix for V5.7. Updates for STEP 7 V17, S7-PLCSIM V17 and WinCC V17Download Hotfix 4 STEP 7 V5.7 / STEP 7 Professional 2021regards sancruz |
Last edited by: sancruz at: 09/27/2022 12:22:40Feedback appreciated, please rate |
|
This contribution was helpful to
1 thankful Users |
1/5/2024 8:31 PM | |
Joined: 1/5/2024 Last visit: 8/3/2024 Posts: 1 Rating:
|
Still occured on Windows 22H2 system with TIA portal V17. ISO deactivation still solved the issue on the network adpater. |
Follow us on