1/8/2024 3:24 PM | |
Joined: 12/17/2018 Last visit: 3/15/2024 Posts: 2 Rating: (0) |
Hello , We have a development Computer for WinCC V8.0. is it possible to install WinCC 7.4 sp1 on the same computer ? |
1/8/2024 4:23 PM | |
Joined: 5/6/2022 Last visit: 5/7/2024 Posts: 416 Rating: (82) |
Hi f.zanouy, It is not possible to install two classic WinCC on one PC. This is because each of the software has its own SQL and cannot coexist together in the same environment. Each of the SQLs needs its own environment. Additionaly: What you can do is to create a MV in the PC and install in it the otrher version. In this way, you can have both versions! Best regards! |
Last edited by: ElonksuM_SN_BN at: 01/08/2024 16:24:31If this Information really helps, you could use the Rate function |
|
This contribution was helpful to2 thankful Users |
Follow us on