Industry Online Support
Technical Forum
1/10/2024 9:52 AM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425)
|
Hi As from TIA V19, it is possible to reset the OB statistics (e.g. longest cycle time, shortest cycle time) using the "RT_INFO" instruction. It is particularly useful for debugging, where it is necessary check the OB cycle time but should necessary to to disregard some special situation (e.g. first scan behaviors) TIPs:
In this sample program a program load could be simulated with instruction wait and RT_INFO could be used to read and reset the OB statistics. Sample project (archived from TIA Portal as .zap19 and after that compacted in .zip format to be uploaded here) user= User, all password = Password1! AttachmentrtInfo.zip (140 Downloads) |
Denilson Pegaia |
|
This contribution was helpful to5 thankful Users |
Follow us on