1/11/2024 10:28 AM | |
Joined: 11/6/2023 Last visit: 1/11/2024 Posts: 1 Rating: (0) |
Hello I set the"Link_1.CAN transparent.Control" to 16#01 in my force table (like the example in the manual above (CAN Transparent table) , which then shows 16#01 in the monitor column which I know is correct and my "Link_1.CAN transparent.Transmit message_1.Int1" messages then show the value I am sending also, so all looks fine (I havent got the Can cable connected yet, waiting on customer) but I have a "Link_1.CAN transparent.Status" of 16#02 and I was wondering where I can see what this actually means - is that ok, error, error no cable connected etc - Is there a list somewhere showing what the return values of this status mean? Just would be nice to know everything is working as expected before i get their can device connected and diagnose any other issues that may arise then Many thanks
|
Last edited by: Jen_Moderator at: 01/12/2024 07:10:45Link optimized. |
|
Follow us on