1/13/2024 2:52 PM | |
Joined: 3/19/2019 Last visit: 4/20/2024 Posts: 92 Rating: (0) |
Hi Alinda, Did you got the solution for this? I'm facing some different issue. Please refer my attachment, Why is "Show-system / Hide-system" messages are showing in status column. If the hide tag value is is 1, that time its displaying the message "hide-system" after that the alarms are hided. Then value changed to 0, that time its displaying message "show-system", after that the alarm are showing. But i don't want to see this "Show-system / Hide-system" in the alarm list. Please let me know how to do this?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/15/2024 11:57:21New subject after splitting "If you want the answer - ask the question" |
|
1/16/2024 12:25 AM | |
Joined: 9/9/2015 Last visit: 4/11/2024 Posts: 727 Rating: (268) |
Hi , I am not 100% sure the question you are asking. You might have already known smart alarm hiding in PCS 7.I will reattach here again for the benefit of the forum user. It should be helpful if you read the document. This is PCS 7 alarm hiding method via logic/condition from programming, by using STrep function block. Attachment55699984_Alarm_Hiding_DOC_PCS7_V90SP1_en.pdf (131 Downloads) |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on