1/23/2024 11:09 AM | |
Joined: 5/6/2022 Last visit: 4/26/2024 Posts: 412 Rating: (81) |
Hi jthyge1, In principle, whether the software version is compatible with the OS is the most important thing. It would also be important to see if you are going to install other components in the OS that may cause incompatibilities. I am attaching the V7.5 SP2 software compatibility so you can see it. Here I also leave you the delivery release of the software where it indicates the compatibility of the Server 2019 OS: "Delivery Release SIMATIC WinCC V7.5 SP2 including options" Best regards! AttachmentWinCC_V7.5_compatibility-list_es_2023-12-19 (1).zip (116 Downloads) |
Last edited by: ElonksuM_SN_BN at: 01/23/2024 11:09:58If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
Follow us on