1/24/2024 8:45 AM | |
Joined: 5/6/2022 Last visit: 5/16/2024 Posts: 420 Rating: (83) |
Hi DamianQS, Below, I comment on all the points to clarify your doubts: 1. The V18 license that you have purchased is an upgrade type, it is not the full license. You must apply this on a complete license such as V14 to convert it to V18. What reference is the upgrade license that you purchased for V18? To tell you if it is valid to apply it. 2. Yes, that is correct. V18 licenses are backward compatible with previous versions. You can see it in the manual: "SIMATIC STEP 7 Basic/Professional V18 and SIMATIC WinCC V18: Licensing STEP 7 and WinCC" 3. I recommend you delete trial licenses that have already expired, since they are no longer valid. 4. In principle, the Trial license must be activated directly. Best regard! |
If this Information really helps, you could use the Rate function |
|
1/24/2024 11:28 AM | |
Joined: 7/9/2015 Last visit: 5/17/2024 Posts: 3833 Rating: (557)
|
Hi, did you check Version of ALM? Install newest Version V6.0 SP12 Upd. 2 Handling programs for authorization or licensing of SIMATIC products (ALM, Authors)Regards, Towome |
|
|
1/29/2024 8:32 AM | |
Joined: 7/6/2022 Last visit: 2/1/2024 Posts: 9 Rating: (0) |
Thank you for your help :-) |
Last edited by: DamianQS at: 01/29/2024 08:33:35 |
|
Follow us on