1/9/2024 6:40 PM | |
Joined: 5/6/2022 Last visit: 5/9/2024 Posts: 419 Rating: (82) |
Hi Swany, It seems a very strange behavior indeed. From what I understand from your post, this problem only happens to you if you have selected/set something giving it a Pallete color, right? If you select a normal non Pallet color, does it show correctly in the Client? What I would recommend to test is to update the version of WinCC V8 to the latest possible version, in case this behavior has been corrected: "Updates for WinCC V8.0 and WinCC V8.0 ASIA" If not I would create an SR to Siemens Support in case it is some kind of bug or something.... Best regards! |
If this Information really helps, you could use the Rate function |
|
This contribution was helpful to1 thankful Users |
2/2/2024 11:59 AM | |
Joined: 6/19/2017 Last visit: 5/10/2024 Posts: 8018 Rating: (163) |
New question published by MustafaQandeel is split to a separate thread with the subject WinCC client shows wrong black color when importing color palettes from the server.. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on