3/1/2024 8:16 PM | |
Joined: 3/14/2008 Last visit: 5/14/2024 Posts: 2066 Rating: (928)
|
Hi, When you click on the small rectangle darker green side in the block in CFC, you will open the runtime sequence editor. In there you see all OB blocks and the runtime groups. All PCS7 blocks must be called in an interrupt OB otherwise the blocks won't be handled properly. Some blocks have additional attributes like being called in OB100. When you insert a block in CFC, the runtime group is automatically created and the block is placed automatically in an interrupt OB and OB100. There are even blocks that need OB80, 81 etc. and those are added automatically as well. I think you moved the block to OB100, I suggest you place it back by using the runtime editor in an interrupt OB3x. An AS compile change and download change must be executed.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on